This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F2800137:如何在 F2800137 Launch Pad 上使用 XDS200U?

Guru**** 2812045 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1411303/tms320f2800137-how-to-use-xds200u-on-f2800137-launch-pad

器件型号:TMS320F2800137

工具与软件:

大家好、团队成员:

如何在 F2800137 Launch Pad 上使用 XDS200U?

我在使用 XDS200测试连接 F2800137:时遇到错误

[Start: Texas Instruments XDS2xx USB Debug Probe_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\a0508909\AppData\Local\TEXASI~1\
    CCS\ccs1271\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
The library build date was 'Apr 19 2024'.
The library build time was '18:50:34'.
The library package version is '12.7.0.00130'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.

An error occurred while hard opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-183' (0xffffff49).
The title is 'SC_ERR_CTL_CBL_BREAK_FAR'.

The explanation is:
The controller has detected a cable break far-from itself.
The user must connect the cable/pod to the target.

[End: Texas Instruments XDS2xx USB Debug Probe_0]

配置如下:

此致、

Zane