工具与软件:
我正在使用2300和4095计数之间的干净1.65V 输入在多个电路板上测量多个 ADC。 计数更有可能接近4095或接近2500、在3000秒内的可能性较低。 在 CCS 中观察测量值的同时、它们会在这个范围内随机摆动。
产生1.65V 电压的硬件已在多个电路板上进行了测量、以确保清洁干净。 我在3个不同的 ADC 引脚上使用有源运算放大器电路和无源分压器创建了此基准电压、结果都是一样的、因此我确信硬件不是问题。
在我的固件中、我使用与示例相同的代码、且每次转换均由软件触发:
//############################################################################# // // FILE: adc_ex1_soc_software.c // // TITLE: ADC Software Triggering // //! \addtogroup driver_example_list //! <h1>ADC Software Triggering</h1> //! //! This example converts some voltages on ADCA and ADCC based on a software //! trigger. //! //! The ADCC will not convert until ADCA is complete, so the ADCs will not run //! asynchronously. However, this is much less efficient than allowing the ADCs //! to convert synchronously in parallel (for example, by using an ePWM //! trigger). //! //! \b External \b Connections \n //! - A0, A1, C2, and C3 should be connected to signals to convert //! //! \b Watch \b Variables \n //! - \b myADC0Result0 - Digital representation of the voltage on pin A0 //! - \b myADC0Result1 - Digital representation of the voltage on pin A1 //! - \b myADC1Result0 - Digital representation of the voltage on pin C2 //! - \b myADC1Result1 - Digital representation of the voltage on pin C3 //! // //############################################################################# // // // $Copyright: // Copyright (C) 2024 Texas Instruments Incorporated - http://www.ti.com/ // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // $ //############################################################################# // // // Included Files // #include "driverlib.h" #include "device.h" #include "board.h" // // Globals // uint16_t myADC0Result0; uint16_t myADC0Result1; uint16_t myADC1Result0; uint16_t myADC1Result1; // // Main // void main(void) { // // Initialize device clock and peripherals // Device_init(); // // Disable pin locks and enable internal pullups. // Device_initGPIO(); // // Initialize PIE and clear PIE registers. Disables CPU interrupts. // Interrupt_initModule(); // // Initialize the PIE vector table with pointers to the shell Interrupt // Service Routines (ISR). // Interrupt_initVectorTable(); // // Set up ADCs, initializing the SOCs to be triggered by software // Board_init(); // // Enable Global Interrupt (INTM) and realtime interrupt (DBGM) // EINT; ERTM; // // Loop indefinitely // while(1) { // // Convert, wait for completion, and store results // ADC_forceMultipleSOC(myADC0_BASE, (ADC_FORCE_SOC0 | ADC_FORCE_SOC1)); // // Wait for ADCA to complete, then acknowledge flag // while(ADC_getInterruptStatus(myADC0_BASE, ADC_INT_NUMBER1) == false) { } ADC_clearInterruptStatus(myADC0_BASE, ADC_INT_NUMBER1); ADC_forceMultipleSOC(myADC1_BASE, (ADC_FORCE_SOC0 | ADC_FORCE_SOC1)); // // Wait for ADCC to complete, then acknowledge flag // while(ADC_getInterruptStatus(myADC1_BASE, ADC_INT_NUMBER1) == false) { } ADC_clearInterruptStatus(myADC1_BASE, ADC_INT_NUMBER1); // // Store results // myADC0Result0 = ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER0); myADC0Result1 = ADC_readResult(ADCARESULT_BASE, ADC_SOC_NUMBER1); myADC1Result0 = ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER0); myADC1Result1 = ADC_readResult(ADCCRESULT_BASE, ADC_SOC_NUMBER1); // // Software breakpoint. At this point, conversion results are stored in // myADC0Result0, myADC0Result1, myADC1Result0, and myADC1Result1. // // Hit run again to get updated conversions. // ESTOP0; } }
我与示例代码的唯一偏差是我仅使用 ADCA、而不是两个 ADC。 我的 syscfg 中可能与此相关的其他设置包括:
ADC 基准电压=内部、2.5V
ADC 时钟预分频器=时钟/4.0
优先级模式=所有轮询
是否有任何已知的 gotcha 可导致固件出现这种行为?