This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F280039C:DCSM

Guru**** 2524550 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1437096/tms320f280039c-dcsm

器件型号:TMS320F280039C

工具与软件:

当我更改 DCSM 的配置以启用 JTAGLOCK 时、不受区域保护的代码。

DCSM 的配置如下:

    

我在使用 CCS 将映像(.out 文件)刷写到 MCU 时遇到错误。

 [错误] C28xx_CPU1:闪存编程期间出错。 地址0x00078028、FMSTAT (在某些器件上为 STATCMD) 0x00001010

这是首次对 OTP 区域进行编程。

;----------------------------------------------------------------------
; Zone 1
;----------------------------------------------------------------------
     .sect "dcsm_otp_z1_linkpointer"
      .retain
      .long 0x00003FFF
      .long 0x00003FFF
      .long 0x00003FFF
    
     .sect "dcsm_otp_z1_jlm_enable"
      .retain
      .long 0xFFFF0000     ;Z1OTP_JLM_ENABLE
     .sect "dcsm_otp_z1_jtag_pswdh"
      .retain
      .long 0x4BFFFFFE     ;Z1OTP_JTAGPSWDH0
      .long 0x3FFFFFFF     ;Z1OTP_JTAGPSWDH1

     .sect "dcsm_otp_z1_cmac_key"
      .retain
      .long 0x2B7E1516     ;Z1OTP_CMACKEY0
      .long 0x28AED2A6     ;Z1OTP_CMACKEY1
      .long 0xABF71588     ;Z1OTP_CMACKEY2
      .long 0x09CF4F3C     ;Z1OTP_CMACKEY3
  
     .sect "dcsm_otp_z1_pswdlock"
      .retain
      .long 0xFB7FFFFF
      
     .sect "dcsm_otp_z1_crclock"
      .retain
      .long 0x7FFFFFFF
   
     .sect "dcsm_otp_z1_gpreg"
      .retain
      .long 0x5AFFFFFF     ;Z1OTP_GPREG1 = Z1_BOOTPIN
      .long 0x5Affffff     ;Z1OTP_GPREG2
      .long 0xFFFFFF0A     ;Z1OTP_GPREG3 = Z1OTP_BOOTDEF_LOW
      .long 0xFFFFFFFF     ;Z1OTP_GPREG4 = Z1OTP_BOOTDEF_HIGH
     .sect "dcsm_zsel_z1"
      .retain
      .long 0xFFFFFF00     ;Z1OTP_CSMPSWD0 (LSW of 128-bit password)
      .long 0x4D7FFFFF     ;Z1OTP_CSMPSWD1
      .long 0xFFFFFFFF     ;Z1OTP_CSMPSWD2
      .long 0xFFFFFFFF     ;Z1OTP_CSMPSWD3 (MSW of 128-bit password)
 
      .long 0xAAAAAAAA     ;Z1OTP_GRABSECT1
      .long 0xAAAAAAAA     ;Z1OTP_GRABSECT2
      .long 0xAAAAAAAA     ;Z1OTP_GRABSECT3
      .long 0x0000AAAA     ;Z1OTP_GRABRAM1
      .long 0xFFFFFFFF     ;Reserved
      .long 0xFFFFFFFF     ;Reserved
 
      .long 0xFFFFFFFF     ;Z1OTP_EXEONLYSECT1
      .long 0x0000FFFF     ;Z1OTP_EXEONLYSECT2
      .long 0x000000FF     ;Z1OTP_EXEONLYRAM1
      .long 0xFFFFFFFF     ;Reserved
      .long 0xFFFFFFFE     ;Z1OTP_JTAGPSWDL0
      .long 0x2BFFFFFE     ;Z1OTP_JTAGPSWDL1    


;----------------------------------------------------------------------

; For code security operation,after development has completed, prior to
; production, all other zone select block locations should be programmed
; to 0x0000 for maximum security.        
; If the first zone select block at offset 0x10 is used, the section 
; "dcsm_rsvd_z1" can be used to program these locations to 0x0000.
; This code is commented out for development.

;       .sect "dcsm_rsvd_z1"
;        .loop (1e0h)
;              .int 0x0000
;        .endloop


;----------------------------------------------------------------------
; Zone 2
;----------------------------------------------------------------------
     .sect "dcsm_otp_z2_linkpointer"
      .retain
      .long 0x00003FFF
      .long 0x00003FFF
      .long 0x00003FFF

     .sect "dcsm_rsvd_z2"
      .retain
      .long 0xFFFFFFFF     ;Reserved
     .sect "dcsm_otp_z2_pswdlock"
      .retain
      .long 0x1F7FFFFF
      
     .sect "dcsm_otp_z2_crclock"
      .retain
      .long 0x3FFFFFFF
            
;;     .sect "dcsm_otp_z2_gpreg"
;;      .retain
;;      .long 0x5AFFFFFF     ;Z2OTP_GPREG1 = Z2_BOOTPIN
;;      .long 0x5AFFFFff     ;Z2OTP_GPREG2
;;      .long 0xFFFFFFCA     ;Z2OTP_GPREG3 = Z2OTP_BOOTDEF_LOW
;;      .long 0xFFFFFFFF     ;Z2OTP_GPREG4 = Z2OTP_BOOTDEF_HIGH
     .sect "dcsm_rsvd1_z2"
      .retain
      .long 0xFFFFFFFF     ;Reserved
      .long 0xFFFFFFFF     ;Reserved

     .sect "dcsm_zsel_z2"
      .retain
      .long 0xFFFFFFFF     ;Z2OTP_CSMPSWD0 (LSW of 128-bit password)
      .long 0x1F7FFFFF     ;Z2OTP_CSMPSWD1
      .long 0xFFFFFFFF     ;Z2OTP_CSMPSWD2
      .long 0xFFFFFFFF     ;Z2OTP_CSMPSWD3 (MSW of 128-bit password)
 
      .long 0xAAAAAAAA     ;Z2OTP_GRABSECT1
      .long 0xAAAAAAAA     ;Z2OTP_GRABSECT2
      .long 0xAAAAAAAA     ;Z2OTP_GRABSECT3
      .long 0x0000AAAA     ;Z2OTP_GRABRAM1
      .long 0xFFFFFFFF     ;Reserved
      .long 0xFFFFFFFF     ;Reserved
 
      .long 0xFFFFFFFF     ;Z2OTP_EXEONLYSECT1
      .long 0x0000FFFF     ;Z2OTP_EXEONLYSECT2
      .long 0x000000FF     ;Z2OTP_EXEONLYRAM1
      .long 0xFFFFFFFF     ;Reserved
      .long 0xFFFFFFFF     ;Reserved
      .long 0xFFFFFFFF     ;Reserved


;----------------------------------------------------------------------

; For code security operation,after development has completed, prior to
; production, all other zone select block locations should be programmed
; to 0x0000 for maximum security.        
; If the first zone select block at offset 0x10 is used, the section 
; "dcsm_rsvd_z2" can be used to program these locations to 0x0000.
; This code is commented out for development.

;       .sect "dcsm_rsvd_z2"
;        .loop (1e0h)
;              .int 0x0000
;        .endloop


;----------------------------------------------------------------------
; End of file
;----------------------------------------------------------------------
/* this linker command file is to be included if user wants to use the DCSM feature on the device
 * DCSM  means Dual Zone Code Security Module.
 * This linker command file works as an addendum ot the already existing Flash/RAM linker command file
 * that the project has.
 * The sections in the *_ZoneSelectBlock.asm source file is linked as per the commands given in the file
 * NOTE - please note fill=0xFFFF, this helps if users include this file in the project by mistake and
 * doesn't provide the needed proper *_ZoneSelectBlock.asm sources .
 * Please refer to the Blinky DCSM example in the controlsuite examples for proper usage of this.
 *
 * Once users are confident that they want to program the passwords in OTP, the DSECT section type can be removed.
 *
*/

MEMORY
{
PAGE 0 :  /* Program Memory */

   /* Z1 OTP.  Z1 password locations / Flash and RAM partitioning */
   DCSM_OTP_Z1_LINKPOINTER     : origin = 0x78000, length = 0x00006
   DCSM_OTP_Z1_JLM_ENABLE      : origin = 0x78006, length = 0x00002
   DCSM_OTP_Z1_GPREG           : origin = 0x78008, length = 0x00008
   DCSM_OTP_Z1_PSWDLOCK        : origin = 0x78010, length = 0x00002
   DCSM_OTP_Z1_CRCLOCK         : origin = 0x78012, length = 0x00002
   DCSM_OTP_Z1_JTAG_PSWDH      : origin = 0x78014, length = 0x00004
   DCSM_OTP_Z1_CMAC_KEY        : origin = 0x78018, length = 0x00008

   /* DCSM Z1 Zone Select Contents (!!Movable!!) */
   DCSM_ZSEL_Z1_P0             : origin = 0x78020, length = 0x000020

   /* Z2 OTP.  Z2 password locations / Flash and RAM partitioning */
   DCSM_OTP_Z2_LINKPOINTER     : origin = 0x78200, length = 0x00006
   DCSM_OTP_Z2_RSVD            : origin = 0x78206, length = 0x00002
   DCSM_OTP_Z2_GPREG           : origin = 0x78208, length = 0x00008
   DCSM_OTP_Z2_PSWDLOCK        : origin = 0x78210, length = 0x00002
   DCSM_OTP_Z2_CRCLOCK         : origin = 0x78212, length = 0x00002
   DCSM_OTP_Z2_RSVD1           : origin = 0x78214, length = 0x0000C
   
   /* DCSM Z2 Zone Select Contents (!!Movable!!) */
   DCSM_ZSEL_Z2_P0             : origin = 0x78220, length = 0x000020

}

SECTIONS
{
   dcsm_otp_z1_linkpointer 	: > DCSM_OTP_Z1_LINKPOINTER		PAGE = 0
   dcsm_otp_z1_gpreg        : > DCSM_OTP_Z1_GPREG		    PAGE = 0
   dcsm_otp_z1_pswdlock		: > DCSM_OTP_Z1_PSWDLOCK		PAGE = 0
   dcsm_otp_z1_crclock		: > DCSM_OTP_Z1_CRCLOCK			PAGE = 0
   dcsm_otp_z1_jlm_enable   : > DCSM_OTP_Z1_JLM_ENABLE,     PAGE = 0
   dcsm_otp_z1_jtag_pswdh   : > DCSM_OTP_Z1_JTAG_PSWDH,     PAGE = 0
   dcsm_otp_z1_cmac_key     : > DCSM_OTP_Z1_CMAC_KEY,       PAGE = 0
   dcsm_zsel_z1				: > DCSM_ZSEL_Z1_P0				PAGE = 0

   dcsm_otp_z2_linkpointer	: > DCSM_OTP_Z2_LINKPOINTER		PAGE = 0
   dcsm_otp_z2_gpreg        : > DCSM_OTP_Z2_GPREG		    PAGE = 0, type = DSECT
   dcsm_otp_z2_pswdlock		: > DCSM_OTP_Z2_PSWDLOCK		PAGE = 0
   dcsm_otp_z2_crclock		: > DCSM_OTP_Z2_CRCLOCK			PAGE = 0
   dcsm_rsvd_z2             : > DCSM_OTP_Z2_RSVD,           PAGE = 0, type = DSECT
   dcsm_rsvd1_z2            : > DCSM_OTP_Z2_RSVD1,          PAGE = 0, type = DSECT
   dcsm_zsel_z2				: > DCSM_ZSEL_Z2_P0				PAGE = 0
}

/*
//===========================================================================
// End of file.
//===========================================================================
*/

在配置 DCSM 时、我需要知道什么问题?

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    你好

    您能否尝试在片上闪存工具中禁用"验证"选项的情况下进行编程? 编程后回读 CSM 密码将导致 DCSM 区域立即被锁定。

    谢谢!

    Luke