This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TMS320F28379D:CLA 不会被触发

Guru**** 2604225 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1477823/tms320f28379d-cla-does-not-get-triggerred

尊敬的专家:

我正在尝试使用 ADCAINT1触发 CLA、但不会被触发! 我甚至使用强制触发器 Cla1Regs.MIFRC.bit.int1 = 1、  但仍然 不会。

请告知我出了什么问题。 这里是项目和代码供您参考。

#include "F28x_Project.h"
#include <math.h>
#include <stdio.h>

#include "Solar_CLA.h"
#include "CLA_Shared.h"

extern void InitSysCtrl(void);
extern void InitPieCtrl(void);
extern void InitPieVectTable(void);
extern interrupt void Cla1Task1();

#define TWO_PI 6.283185307179586476925286766559


interrupt void ADCs_EOC(void);
interrupt void cla_isr(void);

void Initialize_GPIO(void);
void Custom_Init(void);

void PWM1_Init(void);
void Init_ADCs(void);
void X_bar(void);
void InitCla(void);

int buff[100],buff2[100],buff3[100],i,b,c,d,cla=0;
float pi,V_alpha,V_beta,Vd,Vq,R,Y,B,temp,temp2,theta,a=0;


void main(void)
{
   InitSysCtrl();
   Custom_Init();
   PWM1_Init();
   Init_ADCs();

   DINT;
   Initialize_GPIO();
   InitPieCtrl();

   IER = 0x0000;
   IFR = 0x0000;
   InitPieCtrl();
   InitPieVectTable();

   InitCla();



   EALLOW;
   PieCtrlRegs.PIEIER1.bit.INTx1 = 1;    //ADC-A1
   PieCtrlRegs.PIEIER11.bit.INTx1 = 1;  //cla-isr

   PieVectTable.ADCA1_INT = &ADCs_EOC;
   PieVectTable.CLA1_1_INT = &cla_isr;

   PieCtrlRegs.PIECTRL.bit.ENPIE= 1;
   EDIS;

   IER |= 1025;
   EINT;  // Enable Global interrupt INTM
   ERTM;  // Enable Global realtime interrupt DBGM

   while(1)
       {

        }
}
void Initialize_GPIO(void)
{
    EALLOW;
    //GPIO 18 - Xbar input
 /*       GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 0;
    //    GpioCtrlRegs.GPAGMUX2.bit.GPIO18 = 0;
    //    GpioCtrlRegs.GPAPUD.bit.GPIO18 = 1;
   //     GpioCtrlRegs.GPADIR.bit.GPIO18 = 0;
   //     GpioCtrlRegs.GPACSEL3.bit.GPIO18 = 0;
   //     GpioCtrlRegs.GPAQSEL2.bit.GPIO18 = 3;
        InputXbarRegs.INPUT5SELECT = 18;

*/
    // LED out
        GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1;
        GpioCtrlRegs.GPADIR.bit.GPIO31 = 1;
        GpioCtrlRegs.GPCDIR.bit.GPIO73= 1;


   //PWMs
        GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; //ePWM1A


    EDIS;

}
void Custom_Init(void)
{
    EALLOW;
    ClkCfgRegs.CLKSRCCTL1.bit.OSCCLKSRCSEL=1;
    ClkCfgRegs.AUXPLLMULT.bit.IMULT=20;
    ClkCfgRegs.SYSCLKDIVSEL.bit.PLLSYSCLKDIV=0;
    ClkCfgRegs.SYSPLLCTL1.bit.PLLCLKEN = 1;
    ClkCfgRegs.LOSPCP.bit.LSPCLKDIV = 2;
    ClkCfgRegs.PERCLKDIVSEL.bit.EPWMCLKDIV = 0;
    CpuSysRegs.PCLKCR0.bit.CPUTIMER0 = 1;
    CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;   ///source initsysctrl
    CpuSysRegs.PCLKCR2.bit.EPWM1 = 1;
    CpuSysRegs.PCLKCR2.bit.EPWM2 = 1;
    CpuSysRegs.PCLKCR2.bit.EPWM3 = 1;
    CpuSysRegs.PCLKCR2.bit.EPWM4 = 1;
    CpuSysRegs.PCLKCR2.bit.EPWM5 = 1;
    CpuSysRegs.PCLKCR2.bit.EPWM6 = 1;
    CpuSysRegs.PCLKCR2.bit.EPWM7 = 1;
    CpuSysRegs.PCLKCR13.bit.ADC_A = 1;
    CpuSysRegs.PCLKCR0.bit.CLA1 = 1;

    DevCfgRegs.CPUSEL0.bit.EPWM1 = 0;

    EDIS;
}


void ADCs_EOC(void)
{
    EALLOW;
    Cla1Regs.MIFRC.bit.INT1 = 1;
    EDIS;
    Vd=100;
    Vq=0;
    a = AdcaResultRegs.ADCRESULT0; //Va
    temp = (a*62500)/4095;
    EPwm1Regs.CMPA.bit.CMPA = temp;
    EPwm1Regs.CMPB.bit.CMPB = temp + 9000;

    if(i>100)
    {
        i=0;
    }
    theta = TWO_PI*i/100;

    V_alpha = Vd*cos(theta) - Vq*sin(theta);
    V_beta  = Vd*sin(theta) + Vq*cos(theta);

    R =   V_alpha;
    Y = (0.866025*V_beta)-(0.5*V_alpha);
    B = -(0.5*V_alpha)-(0.866025*V_beta);

    buff2[i] = R;
    buff[i]= Y;
    buff3[i]= B;
    i= i+1;

    EPwm1Regs.ETCLR.bit.SOCA = 1;
    AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //clear INT1 flag
    PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}

void cla_isr(void)
{
    cla=cla+1;
    if(cla>10)
    {
        cla = 0;
    }
    AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //clear INT1 flag
    Cla1Regs.MCTL.bit.IACKE = 1;
    PieCtrlRegs.PIEACK.all = PIEACK_GROUP11;
}

void PWM1_Init(void)
{
          EALLOW;
          //R Phase
          EPwm1Regs.TBCTL.bit.CTRMODE = 0;             // Count up
          EPwm1Regs.TBPRD = 62500;                    // Set timer period
          EPwm1Regs.TBCTL.bit.PHSEN = 0;               // 1 for external SYNC
          EPwm1Regs.TBPHS.bit.TBPHS = 0x0000;          // Phase is 0
          EPwm1Regs.TBCTR = 0x0000;                    // Clear counter
          EPwm1Regs.TBCTL.bit.HSPCLKDIV = 2;           // Clock ratio to SYSCLKOUT
          EPwm1Regs.TBCTL.bit.CLKDIV = 4;
          EPwm1Regs.TBCTL.bit.SYNCOSEL = 1;
          // Setup shadow register load on ZERO
          EPwm1Regs.CMPCTL.bit.SHDWAMODE = 0;
          EPwm1Regs.CMPCTL.bit.SHDWBMODE = 0;
          EPwm1Regs.CMPCTL.bit.LOADAMODE = 0;
          EPwm1Regs.CMPCTL.bit.LOADBMODE = 0;
          // Set Compare values
                // Set compare A value
          // Set actions
          EPwm1Regs.AQCTLA.all = 0;
          EPwm1Regs.AQCTLA.bit.CAU = 2;                // Set PWM1A on TBCTR = CMPA
          EPwm1Regs.AQCTLA.bit.CBU = 1;                // Clear PWM1A on TBCTR = CMPB= CMPA + 100


          //SOCA to ADC
          EPwm1Regs.ETSEL.bit.SOCAEN=1;
          EPwm1Regs.ETSEL.bit.SOCASEL=1;
          EPwm1Regs.ETPS.bit.SOCAPRD = 1;
          EPwm1Regs.ETCLR.bit.SOCA = 1;

          EDIS;
}

void InitCla(void)
{
    EALLOW;
    DevCfgRegs.DC1.bit.CPU1_CLA1 = 1;

    Cla1Regs.MCTL.bit.HARDRESET = 1;
    Cla1Regs.MCTL.bit.SOFTRESET = 1;
    Cla1Regs.MCTL.bit.IACKE     = 1;
    Cla1Regs.MIER.bit.INT1      = 1; //enable Task1
    Cla1Regs.MVECT1 = (uint16_t)(&Cla1Task1);  //vector address
    Cla1Regs.MICLROVF.bit.INT1 = 1;

    MemCfgRegs.LSxMSEL.all = 0;
    MemCfgRegs.LSxCLAPGM.all=0;
    MemCfgRegs.LSxMSEL.bit.MSEL_LS0     = 1; //LS0 for CLA 8000 to 87FF (2K words) more than enough I guess for now
    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS0 = 1; //LS0 for program memory
    MemCfgRegs.LSxMSEL.bit.MSEL_LS1     = 1; //LS1 for CLA 8800 to 8FFF (2K words)
    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS1 = 0; //LS1 for Data memory

    DmaClaSrcSelRegs.CLA1TASKSRCSEL1.bit.TASK1 = 1; //ADCAINT1

    EDIS;

}


void Init_ADCs(void)
{
            EALLOW;

            AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1;
            AdcbRegs.ADCCTL1.bit.INTPULSEPOS = 1;
            AdccRegs.ADCCTL1.bit.INTPULSEPOS = 1;

            AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1;
            AdcbRegs.ADCCTL1.bit.ADCPWDNZ = 1;
            AdccRegs.ADCCTL1.bit.ADCPWDNZ = 1;
   //         DELAY_US(1);

            AdcaRegs.ADCCTL2.bit.PRESCALE = 6;
            AdcbRegs.ADCCTL2.bit.PRESCALE = 6;
            AdccRegs.ADCCTL2.bit.PRESCALE = 6;

            AdcaRegs.ADCSOC0CTL.bit.CHSEL = 0;  //SOC0 will convert pin A0
            AdcaRegs.ADCSOC1CTL.bit.CHSEL = 1;  //SOC1 will convert pin A1
            AdcaRegs.ADCSOC2CTL.bit.CHSEL = 2;  //SOC2 will convert pin A2
            AdcaRegs.ADCSOC3CTL.bit.CHSEL = 3;  //SOC3 will convert pin A3
            AdcaRegs.ADCSOC4CTL.bit.CHSEL = 4;  //SOC4 will convert pin A4
            AdcaRegs.ADCSOC5CTL.bit.CHSEL = 5;  //SOC5 will convert pin A5


            AdcaRegs.ADCSOC0CTL.bit.ACQPS = 14; //sample window is 100 SYSCLK cycles
            AdcaRegs.ADCSOC1CTL.bit.ACQPS = 14; //sample window is 100 SYSCLK cycles
            AdcaRegs.ADCSOC2CTL.bit.ACQPS = 14; //sample window is 100 SYSCLK cycles
            AdcaRegs.ADCSOC3CTL.bit.ACQPS = 14; //sample window is 100 SYSCLK cycles
            AdcaRegs.ADCSOC4CTL.bit.ACQPS = 14; //sample window is 100 SYSCLK cycles
            AdcaRegs.ADCSOC5CTL.bit.ACQPS = 14; //sample window is 100 SYSCLK cycles


            AdcaRegs.ADCBURSTCTL.bit.BURSTEN = 1;
            AdcaRegs.ADCBURSTCTL.bit.BURSTSIZE = 11;
            AdcaRegs.ADCBURSTCTL.bit.BURSTTRIGSEL = 5;



            //interrupt
            AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 0; //end of SOC0 will set INT1 flag
            AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1;   //enable INT1 flag
            AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //make sure INT1 flag is cleared
            AdcaRegs.ADCSOC1CTL.bit.TRIGSEL = 05;

    EDIS;
}

e2e.ti.com/.../4857.blink.zip

此致、

Rajesh。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我在这方面做了一些改进!

    我添加了"memcpy (&Cla1funcsRunStart、&Cla1funcsLoadStart、(uint32_t)&Cla1funcsLoadSize);"以在启用了 CLA 的 RAM 部分上加载 CLA 任务。

    现在我看到变量执行了 ADC_ISR CLA  但 CLATASK 中的变量 T、  不会递增、尽管出现行" T+1 "

    此致、

    Rajesh。