Other Parts Discussed in Thread: LMX2595
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:LMX2595 大家好,
我在设计中使用LMX2595,我想使用输入参考时钟单端。 我有一个外部时钟信号CMOS (3.3V,10MHz),但我在数据表中读过
在6.5 中 ,电气特性最大电压为2Vpp。 我想问我是否可以将此时钟用于LMX2595?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.