This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LMX2594EVM:LMX2594EVM输出功率问题

Guru**** 2595805 points
Other Parts Discussed in Thread: LMX2594EVM

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/clock-timing-group/clock-and-timing/f/clock-timing-forum/648400/lmx2594evm-lmx2594evm-output-power-issue

部件号:LMX2594EVM

您好,

我们没有足够的LMX2594EVM输出功率(根据数据表)。

使用18nH和1nH上拉电感器以及50欧姆上拉电阻器执行单端测量。 与规格相比的测量结果如下图所示(电缆损耗已解除嵌入):

要在8GHz - 10GHz和12GHz-14GHz频率范围内实现最大输出功率,您建议使用什么?