请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TPL5110 在TPL5110的数据表中,"TPL5110可以在100ms到7200s范围内生成1650离散计时器间隔。 前9个间隔是100ms的倍数。 剩余的1641间隔涵盖1至7200秒的范围。"
我想知道确切的"剩余1641个间隔"是什么?
如果1641时间间隔是固定的,我是否仍然可以配置任何时间间隔,如30分钟35秒500毫秒?
提前感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.