请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:LMX2581E 您好,
在数据表中,V_IH的额定电压为1.4V至Vcc。 从我的FPGA来看,LVCMOS18 VOH最小值为Vcc-0.45V,对于我的应用来说,为1.8V-0.45V=1.35V。 我想知道SPI控制电压是否可以支持最低为1.35V的V_IH电压。或者如果这太低,我们需要电平转换器来支持这种电压。您可以建议吗?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
在数据表中,V_IH的额定电压为1.4V至Vcc。 从我的FPGA来看,LVCMOS18 VOH最小值为Vcc-0.45V,对于我的应用来说,为1.8V-0.45V=1.35V。 我想知道SPI控制电压是否可以支持最低为1.35V的V_IH电压。或者如果这太低,我们需要电平转换器来支持这种电压。您可以建议吗?
谢谢