请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LMK04832 大家好、团队、
您能否告诉我 SPI 引脚的绝对最大电压/电流额定值?
我想确认、如果 SPI 引脚出现1.8V 过压但电流限制在700uA 以内、LMK04832将损坏。
此致、
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.