请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LMX2594 Thread 中讨论的其他器件:LMX2491
您好!
能否在200us 内生成5.8GHz 至6GHz 范围内的连续锯齿波形输出频率?
此致
Sushant
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.