请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LMX2594 主题中讨论的其他器件:LMX2820
我想知道突发模式是如何工作的?
我想生成1us 宽度的脉冲,其频率为200MHz。 与 FSK 调制类似,载波频率为0和100MHz,这取决于外部触发器。 可以吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.