请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:FDC2214您好、支持团队、
我的客户正在寻找从电容到 PWM 时钟的转换产品。 请告诉我您的建议。
电容范围:1pF 至50pF
预期输出频率:150或160kHz 至200kHz。 (1kHz/1pF)
谢谢、
Koji Ikeda
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.