Other Parts Discussed in Thread: LMC555
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:LMC555大家好、
时钟生成/缓冲器是否可用于100Hz 至1KHz 或10kHz 的 PWM 信号?
如果是、建议使用哪一部分?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.