请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LMK03328 错过另一个100MHz 频率、因此我们需要4种不同的频率:307.2MHz、156.25MHz、125MHz 和100MHz。 请确认 LMK03328是否 可以生成这4个频率?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
错过另一个100MHz 频率、因此我们需要4种不同的频率:307.2MHz、156.25MHz、125MHz 和100MHz。 请确认 LMK03328是否 可以生成这4个频率?