Other Parts Discussed in Thread: LMK1C1104, SN3257-Q1, TMUX136, TMUX6119
主题中讨论的其他器件: SN3257-Q1、 TMUX136、 TMUX6119
寻找一个 SPDT 开关 、将 COM 连接到 LMK1C1104的 CLK 输入、用于1.8V 和3.3V LVCMOS。
如果输入可耐受5V 电压、则效果会更好。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好 Lauri、
明白了! 因此、一个好的做法是选择带宽为所需带宽的1.5倍的器件。 我看到 LMK1C1104的最大频率为250MHz。 因此、对于在1.8V、3.3V 和高达5V 时支持至少375MHz 频率的单通道开关、如果您可以在双轨模式下使用 TMUX6119、则它是唯一的选择。 如果双轨不是所需的应用、那么我们需要查看可以支持单轨的双通道多路复用器选项、在这种情况下、TMUX136是一个很好的选择。
谢谢!
Alex