Other Parts Discussed in Thread: LMX2582
您好!
我们面临与 LMX2582锁定检测有关的问题。
锁定检测指示 PLL 处于锁定状态、即使不处于锁定状态(输出频率不正确)。
我们如何才能解决该问题?
谢谢。
罗内尔
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
输入 CLK 由50MHz VTCXO 参考提供、器件型号- LFVCXO066860Bulk。
我想 说明的是、当 PLL 处于锁定状态时、它提供了良好的 PN 性能-从1kHz 到100MHz 的积分为51dBc。
配置为:
R70 0x460000
R69 0x450000
R68 0x440489
R64 0x400377
R62 0x3E0000
R61 0x3D0000
R59 0x3B0000
R48 0x3003FC
R47 0x2F08C0
R46 0x2E1FA3
R45 0x2D0003
R44 0x2C0000
R43 0x2B000B
R42 0x2A0000
R41 0x29000A
R40 0x280000
R39 0x278204
R38 0x260024
R37 0x254000
R36 0x240811
R35 0x23021B
R34 0x22C3EA
R33 0x212A0A
R32 0x20210A
R31 0x1F0401
R30 0x1E00F4
R29 0x1D0084
R28 0x1C2924
R25 0x190000
R24 0x180509
R23 0x17B042
R22 0x162300
R20 0x14012C
R19 0x130965
R14 0x0E0FFC
R13 0x0D4000
R12 0x0C7001
R11 0x0B0018
R10 0x0A10D8
R9 0x090B02
R8 0x081084
R7 0x0728B2
R4 0x041943
R2 0x020500
R1 0x01080A
R0 0x00221C