我在windows i上使用ccs11 tirtos 520
并从 资源管理器中导入新的软件cc1312 emtpy项目TIRTOS。
一旦我建立了它,它就会持续显示以下错误
**** Build of configuration Debug for project tirtos_builds_cc13x2_cc26x2_release_ccs_5_20_00_52 **** "C:\\ti\\ccs1110\\ccs\\utils\\bin\\gmake" -k -j 8 all -O Building file: "../release.cfg" subdir_rules.mk:12: recipe for target 'build-1231611761-inproc' failed '0' is not recognized as an internal or external command, operable program or batch file. gmake[1]: *** [build-1231611761-inproc] Error 1 Building file: "../release.cfg" subdir_rules.mk:12: recipe for target 'build-1231611761-inproc' failed '0' is not recognized as an internal or external command, operable program or batch file. gmake[2]: *** [build-1231611761-inproc] Error 1 makefile:127: recipe for target 'all' failed gmake[1]: *** No rule to make target 'build-1231611761', needed by 'configPkg/linker.cmd'. gmake[1]: Target 'configPkg/linker.cmd' not remade because of errors. gmake: *** [all] Error 2 **** Build Finished ****

如果有任何解决方案请提出建议。谢谢