请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DAC37J84 当我对DAC进行编程以输出Block0 PLL时钟/80时,似乎没有从报警引脚中得到任何东西。
我通过写入0x0100到SPI上的0x1b地址来执行此操作。
我的SerDes PLL应以2.4GHz运行,因此我希望在报警引脚外看到30MHz。
是否需要配置其它寄存器才能使PLL时钟超出报警引脚?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
当我对DAC进行编程以输出Block0 PLL时钟/80时,似乎没有从报警引脚中得到任何东西。
我通过写入0x0100到SPI上的0x1b地址来执行此操作。
我的SerDes PLL应以2.4GHz运行,因此我希望在报警引脚外看到30MHz。
是否需要配置其它寄存器才能使PLL时钟超出报警引脚?