This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
尊敬的:
我们 的设备模拟信号采样电路使用ADS7830,输入测量电压范围为0~5V。 现在,我有几个关于ADS7830的问题:
1.由于输入测量电压范围为0~5V,因此电源电压+VDD必须为5V?
2.REF输入/ REF 输出引脚直接连接至5V电源电压?
3.如何处理COM引脚? 连接到GND?
4.如果电源电压+VDD为5V,那么I2C接口电平是否变为5V? 在这种情况下,我们打算使用 PCA9306来调整使用3.3V电源电压的CPU的I2C接口。 TI 是否推荐此连接方法?
5.如何处理模拟输入的EMC? TI是否有 参考 设计?
谢谢,我将等待您的回复。