请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:ADS1675 您好,
当DRATE为'001'(250kHz)和'101'(4MHz)时,您能否提供低延迟,快速响应模式的滤波系数?
ADC:ADS1675
模式:低延迟,快速响应
DRATE:001 / 101
原因:ADC 建模
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.