主题中讨论的其他部件: DAC38RF82
大家好,
我正在尝试在12位时钟模式(CMODE5)中使用DAC38RF82EVM。 根据EVM用户指南(第4页,1.5 节),它需要在1.2 J1和上分别使用两个时钟。 但是,对于如何确定SMA J1和J4上每个时钟的频率尚不清楚。 我已尝试启用片上PLL,设置参考频率= 375M,M=4,N=1,时钟(J4)=1.5G以及提供的外部时钟(J1)=6G,但此设置不起作用。
此致,
SAAD
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,
我正在尝试在12位时钟模式(CMODE5)中使用DAC38RF82EVM。 根据EVM用户指南(第4页,1.5 节),它需要在1.2 J1和上分别使用两个时钟。 但是,对于如何确定SMA J1和J4上每个时钟的频率尚不清楚。 我已尝试启用片上PLL,设置参考频率= 375M,M=4,N=1,时钟(J4)=1.5G以及提供的外部时钟(J1)=6G,但此设置不起作用。
此致,
SAAD
Saad,
执行以下操作:
1.为J1提供375MHz。
2.为J4提供281.25MHz。
3.对发援会进行编程
4.转至DAC38RF8x计时选项卡,并将外部时钟选择设置为SE路径。
5.转至LMK时钟输出选项卡,将CLK0和1除法器更改为“1”,并将 DCLK源设置为除法器+ DCC + HS
6.在“快速启动”选项卡上,单击“PLL自动调谐”。
7.加载TSW14J56固件并提供测试文件。
此致,
Jim