Other Parts Discussed in Thread: ADS7863A
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:ADC122S655 主题中讨论的其他部件:ADS7863A
是否有类似的部件可用,但能够在3V或3.3V电源下工作?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS7863A
是否有类似的部件可用,但能够在3V或3.3V电源下工作?
你(们)好
如果您特别需要12位分辨率,我建议您查看ADS704x系列。 您可以使用两个ADS704x。 您可以 将 每个ADC (CS)的芯片选择引脚连接在一起,并使用相同的时钟进行转换。 因此您需要4条数字线路
1.芯片选择(两个ADC相同)
2.时钟(两个ADC的时钟相同)
3.单个ADC的SDO1和SDO2
请告诉我这种方法是否正常
谢谢,顺祝商祺
Abhijeet