请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:AMC7832 在AMC7832中,ADC可以采用-12.5V到12.5V范围内的输入电压,它将通过采用2.5V参考将此I/p电压转换为数字电压。但问题是它如何将-12.5V 到12.5V范围内的电压转换为12位输出?我想知道 从 -12.5V到12.5V的电压转换为12位双元形式。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.