请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DAC3484 团队成员,您好!
我支持使用DAC3484的应用程序,是否需要在更改输入时钟速度时更改任何设置? (假设从122.88 MHz到153.6 MHz)
如果是,是否有任何说明这一点的文档?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.