Other Parts Discussed in Thread: ADS124S08
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:ADS124S08 大家好,
我绕过PGA,将AINCOM连接到+2.5V (以AINN的形式),内部参考,AINps的范围从0~5V,我想知道AINCOM 的输入阻抗,有人可以告诉我在哪里找到它?
黄先生。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.