德拉斯,
我的客户对数据表中的带宽有一些疑问。
表8中提到生物武器,其定义是什么?
例如,BW是160,它是menas
A.信号只能在0~160Hz范围内传递
B.信号只能从0.05~160Hz传输
c.信号只能从0.5~160Hz或传送
D.其他,请加以解释
2.基于上述问题,如果客户想要设计0~150Hz LPF,他们需要怎么做?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好Peter,
感谢您对我们的ADS1293的关注!
表8中列出的带宽是PACE和ECG通道数字滤波器输出的信号带宽。 此带宽取决于抽取比率和输出数据速率。 通常,此规范指示数字滤波器响应的-3dB点。
如果您回顾图18,您会发现数字滤波器由三个阶段组成,每个阶段都是一个具有不同小数比的sinc5滤波器。 PACE通道来自第2阶段的输出,而ECG通道来自第3阶段的输出。 根据输出的来源,滤波器响应看起来会有所不同,但所有响应都将从DC处的单位增益(0 dB)开始,然后在表8中指定的信号带宽处滚动到-3 dB。
客户是否只对0赫兹到150赫兹的信号感兴趣? 我仍然认为数字滤波器中的160Hz带宽就足够了-请记住,滤波器响应将在-3dB点之前开始滚动,因此实际上,您希望滤波器截止值超出您感兴趣的信号带宽。 否则,如果他们希望-3dB点精确出现在150Hz,则可以调整输入时钟频率。 可接受的输入时钟频率范围为3.7MHz至4.5MHz。 有关ADS1293时钟选项的更多详细信息,请参阅第28页上的第8.3 .................................................................19节。
此致,