请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:PGA308 TI 工程师:您好
当我们调试PGA308时,我们发现当VS=3.34V,VREF=3.25V时,寄存器ZDAC和GDAC可以写入 数据,但我们读取了其它数据!
当VS电压调整为3.27V电压时,寄存器ZDAC和GDAC可以读取和写入相同的数据。
VS和VREF电压之间的对应关系是什么?这如何影响1W的寄存器读写? 或者1W的计时是否有问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.