Other Parts Discussed in Thread: ADS1115, ADCPRO, ADS1015
在“线程: ADCPro, ADS1015”中讨论的其他部件
尊敬的专家:
ADS1115似乎没有可用的EVM。 由于1115是P2P与1015,是否可以在1015 EVM上使用1115? 如果将EVM上的1015替换为1115,EVM是否仍可与PDK一起使用,以及它是否仍与ADCPro兼容?
谢谢!
Rgds,
Juha
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
胡哈
ADS1115EVM已过时。 ADS1015也在该过程中。 ADCPro是在Windows XP的时代设计的,现在只能在Windows 7上运行(尽管我认为人们已经获得了它来在更高版本上工作)。 我们正在开发基于MSP430 Booster Pack的替换产品,该产品将于明年推出。
同时,ADS1115EVM仍可在某些供应商处获得。 我可以在Digikey上找到它:
此外,还可以使用ADS1015EVM评估ADS1115的基本功能。 EVM仍可从TI获得:
最后,您可以使用I2C仿真器并直接从简单的电路板驱动ADS1115。 Adafruit制造了相对便宜的ADS1115电路板:
对此造成的不便,我们深表歉意。
吴若瑟