This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
我正在使用模数转换器芯片ADS1298来记录弱生物信号。 我想在ADS1298芯片之前引入一个仪表放大器芯片,以便为我的系统实现更好的输入参考噪声。
我的ADS1298芯片电源是:VREFP=+2.5V, VREFN=-2.5V和DVDD=+3.3V。
我的问题是,在ADS1298芯片之前,我要介绍的仪表放大器是否必须与ADS1298芯片具有相同的电源(+-2.5V)。
换句话说,您是否认为在 ADS1298之前引入具有+-5V电源的仪表放大器会对 ADS1298 转换器的功能造成任何问题?
提前感谢您的参与,
Konstantinos
Tom,您好!
非常感谢您的及时回复!
我完全理解您的顾虑。
但是,由于ADS1298是一种AFE芯片,其PGA先于实际ADC部件,因此我预计这些PGA将在输入电压变为+/- 5V时进行剪辑,并保护实际ADC部件(随+/-2.5V提供)。
我是正确的,还是遗漏了什么?
再次感谢您的帮助,
Konstantinos