请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:ADS7142 我刚刚收到了BOOSTXL-ADS7142评估平台,并注意到在自主模式和i2c模式下运行时,ADC读数不同。
例如: 在I2C模式下对CH0应用2V输入,可获得 2525的ADC读数,但当切换到自主模式时,ADC值为2458 -差值约为50mV。
有没有解释为何会出现这种情况?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.