请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DAC38J84 我正在使用DAC38j84生成Fo=800MHz,BW=100MHz芯片信号,变压器ADTL2-18可输出信号结束的波形。
需要使用LC滤波器来过滤镜像,我的问题是:
我应该在变压器之前使用差分LC滤波器,还是在ADTL2-18之后使用信号端LC滤波器?在实际应用中,这更好?为什么?
期待您的回复
谢谢
哇
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.