请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:ADS1675 您好,我发现我正在使用的DSP没有LVDS。
我看到ADS1675具有DOUT和/DOUT,它们将用于LVDS模式? 如果我在标准CMOS模式下使用IC,这是否意味着我只需要使用DOUT,而不是/DOUT?
谢谢!
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.