Other Parts Discussed in Thread: ADS4149, ADS4149EVM
你(们)好
ADS4149 VCM 在上电后不稳定、从0.9更改为0.4V、仍然不保持0.95V、这是什么情况?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS4149, ADS4149EVM
你(们)好
ADS4149 VCM 在上电后不稳定、从0.9更改为0.4V、仍然不保持0.95V、这是什么情况?
您好、Jim、
删除 R22、R23、C32、C141、VCM 后仍然不稳定。(0.26~0.67V)
我有一个问题、即 VCM 是否需要写入寄存器命令、通常情况下、VCM 输出应改变上电
我发现 addr=03H/Data=03H、VCM 为1.1V、电压稳定、我不知道为什么需要控制 VCM?如何 生成 VCM
图70. 寄存器地址03h 高性能模式1
位7-2始终写入0
位1-0高性能模式1:高性能模式1
00 =复位后的默认性能
01 =请勿使用
10 =请勿使用
11 =为了在采样时钟和输入信号频率范围内获得最佳性能、请设置高性能
模式1位
此致、
Charlie