Other Parts Discussed in Thread: ADS8634, ADS8364
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:ADS8634、 ADS8364您好、社区
请为 ADC IC 器件提供以下参数。
由+5V 和-5V 双电源供电
单端输入通道。
采样率= 10-50 MSPS
12位 ADC
谢谢、此致、
Divya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.