请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:ADS1258 主题中讨论的其他器件:ADS1241、
大家好! 我有一个简单的问题:ADS1258数据表中名为 XTAL1、XTAL2的 XTAL 引脚;谁是谁、输入/输出? 在新设计中、我希望将串联电阻器放置在32768Hz 晶体上、与 ADS1241数据表中的相同。
BR、Nick。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.