Other Parts Discussed in Thread: ADC3422
您好!
在数据表中、直流精度见下表。
因此、如果使用此 ADC3422来测量2V 输入电压、
最坏情况下的误差将是、25mV 偏移和2% FS = 40mV
因此、总误差将为25mV+40mV = 65mV。
请告诉我上述理解是否正确?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
我与我的一位同事谈到过、您需要对失调电压、增益和漂移误差进行 RSS 处理。 请参阅以下文章:
此致、Amy