This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ADC3422:ADC 的直流准确度

Guru**** 2928980 points

Other Parts Discussed in Thread: ADC3422

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1205916/adc3422-the-dc-accuracy-of-adc

器件型号:ADC3422

您好!

在数据表中、直流精度见下表。

因此、如果使用此 ADC3422来测量2V 输入电压、

最坏情况下的误差将是、25mV 偏移和2% FS = 40mV

因此、总误差将为25mV+40mV = 65mV。

请告诉我上述理解是否正确?