Other Parts Discussed in Thread: DAC8775
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DAC8775 我当前的 DAC8775发热较高、如何实现自适应电源管理功能?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
您可以通过写入寄存器0x06 (选择 Buck-Boost)和0x07 (配置 Buck-Boost)来使用降压/升压转换器。
当 CCLP ="00"时、缺省模式允许降压-升压转换器自适应地改变正负输出。
要激活降压/升压转换器、请通过写入寄存器0x06来选择相应的 PNSEL、然后将寄存器0x07中的 PNSEL 设置为"11"、以便同时启用正负输出。
数据表的第8.3.3节 更详细地介绍了每个可能的设置。
谢谢。
卢卡斯