Other Parts Discussed in Thread: DAC3482
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DAC3482 您好
我能否为 数据速率为500MHz 且输出采样率为1.25Gsps 的 DATACLK 和 DACCLK 提供250MHz 时钟?
如果可能,我应该如何配置设备?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.