工具与软件:
您好、我正在从 ADS8681读取寄存器值。 我得到的值 DEVICE_ID_REG 寄存器(地址= 0x0) 为0x10。 我认为它的默认值是0。 为什么会这样? 数据表是否过时?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
无论我是从读取8位还是16位 DEVICE_ID_REG 寄存器(地址= 00h) 时、为 bits[15:0]返回的值仍为0x10、 而不是0x0。
今天、我已经确认我的 SPI 写入/读取函数都可以正常工作。 我通过将0xb 写入来验证 RANGE_SEL_REG 寄存器(14h) 并且能够读回0xb。
ADS8681数据表是否过时?
ADS868x 具有可编程双极输入范围的16位、高速、单电源 SAR ADC 数据采集系统数据表(修订版 E)