请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC28740 工具与软件:
您好!
查看数据表、Vocp 为1.4~1.6V (-40~125℃)。
Vocp 是否具有随着温度升高阈值变小(接近1.4V)的特征?
谢谢!
Conor
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具与软件:
您好!
查看数据表、Vocp 为1.4~1.6V (-40~125℃)。
Vocp 是否具有随着温度升高阈值变小(接近1.4V)的特征?
谢谢!
Conor