This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] ADS1261:配置寄存器的回波被1关闭

Guru**** 2918620 points

Other Parts Discussed in Thread: ADS1261

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/1475817/ads1261-echo-of-configuration-register-is-off-by-one

器件型号:ADS1261

工具与软件:

大家好!

发送 RESET 命令以及配置 PGA、INPMUX 和基准电压时、地址回波会熄灭、我会遇到此问题。这三种配置和 One 命令每次都会发生此问题。 此外、寄存器值看起来不正确、因为(LSB)始终设置为高电平。 我已经使用逻辑分析仪来验证信号、微控制器正在发送正确的信号。 不过、我将获得 ADC 读数、例如、ADC 报告的电压为1.948V、而测量值为2.175V。

我使用的是 Arduino 框架和 Espressif ESP32-S3-DevKitC-1-N32R8V。

对于 SPI 模式、我选择了 SPI_MODE 1 (CPOL = 0、 CPHA = 1)、我尝试的 SPI CLK 速度在100kHz 至9MHz 之间变化、输出仍然相同。

以下是 C++代码片段:

ADS1261::ADS1261() : SPI_Instance(SPI0_Selector, (SPI_Chipselect)ADS1261_nCS, DataMode_1) {
    
    // Configure GPIOs
    pinMode(ADS1261_nReset, OUTPUT);
    pinMode(ADS1261_nPWDN, OUTPUT);
    pinMode(ADS1261_START, OUTPUT);
    pinMode(ADS1261_nCS, OUTPUT);
    pinMode(ADS1261_nDRDY, INPUT);

    digitalWrite(ADS1261_nReset, HIGH);  // Bring reset HIGH
    digitalWrite(ADS1261_nPWDN, HIGH);   // Power up ADC
    digitalWrite(ADS1261_nCS, LOW);      // Deselect ADC

    // Hardware Reset Sequence
    Serial.printf("Waiting for DRDY to be LOW\n");
    while(digitalRead(ADS1261_nDRDY) != HIGH){
        delayMicroseconds(100);
    }
    Serial.printf("DRDY is LOW\n");
    SendCommand(0xF5,0x00);
    digitalWrite(ADS1261_START, LOW);
    
    delay(60);
    Serial.println("ADS1261 Initialization Started...\n");

    bool Success = true;
    uint8_t Val = 0;

    Serial.println("Sending RESET command...\n");
    digitalWrite(ADS1261_nCS, LOW);
    delayMicroseconds(100);
    Success &= SendCommand(0x06, 0xAA);
    delayMicroseconds(300);

    // Unlock Registers
    SendCommand(0xF5,0x00);
    delayMicroseconds(300);
    Serial.println("Configuring ADC Registers...\n");
    
    /*
    MODE1: 
    Currently in Chop mode and 17.8ms start delay 
    also tested with Normal mode, Continous mode with 50 microseconds 
    */
    Success &= SetRegister(0x03, 0x2D);  // tested with 0x10 and 0x2D
    delayMicroseconds(1000);
    GetRegister(0x03,&Val);
    Serial.println("---------------------------");
    Serial.printf("Read Value: 0x%x\n",Val);
    Serial.println("---------------------------");
    delayMicroseconds(100);
        /*
        PGA
        In Bypass mode
        Gain: 1
        */
    Success &= SetRegister(0x10, 0x00);
    delayMicroseconds(100);
    GetRegister(0x10,&Val);
    Serial.println("---------------------------");
    Serial.printf("Read Value: 0x%x\n",Val);
    Serial.println("---------------------------");
    delayMicroseconds(100);


    /*
    Internal Reference Voltage:
    Internal Reference enabled
    Internal ref. positive and negative
    */

    Success &= SetRegister(0x06, 0x10); //also tested with 0x15
    delayMicroseconds(100);
    GetRegister(0x06,&Val);
    Serial.println("---------------------------");
    Serial.printf("Read Value: 0x%x\n",Val);
    Serial.println("---------------------------");
    delayMicroseconds(2000);

    /*
    INPMUX: 
    Postive Input: AIN0
    NegativeInput: AINCOM
    */
    Success &= SetRegister(0x11, 0x10);
    delayMicroseconds(100);
    GetRegister(0x11,&Val);
    Serial.println("---------------------------");
    Serial.printf("Read Value: 0x%x\n",Val);
    Serial.println("---------------------------");
    delayMicroseconds(100);

    digitalWrite(ADS1261_START, HIGH);

    Serial.println("Waiting for DRDY to be LOW...");
    while(digitalRead(ADS1261_nDRDY) != HIGH){
        delayMicroseconds(100);
    }
    Serial.println("DRDY is LOW");
    

    if (!Success) {
        Serial.println("Failed to initialize ADC registers!\n");
    } else {
        Serial.println("ADS1261 Initialization Successful!\n");
    }
}

bool ADS1261::SetRegister(uint8_t const Address, uint8_t const Value)
{
    const uint8_t WREGCommand = 0x40;
    return SendCommand(WREGCommand + (Address & 0x1F), Value); // taken from the example code of TI
}

bool ADS1261::SendCommand(uint8_t const Command, uint8_t const Data)
{
    const uint8_t BufferLen = 2;
    uint8_t const WriteBuffer[BufferLen] = {Command, Data};
    uint8_t ReadBuffer[BufferLen] = {0};


    delayMicroseconds(10);
    bool Success = SPI_Instance.ReadWrite(WriteBuffer, ReadBuffer, BufferLen);
    
    Serial.println("---------------------------------------------------------");
    Serial.printf("Sent Command: 0x%X 0x%X\n", WriteBuffer[0], WriteBuffer[1]);
    Serial.printf("Received Response: 0x%X 0x%X\n", ReadBuffer[0], ReadBuffer[1]);
   
    if(Command == 0x06){
        delay(10);
    }

    Success &= ReadBuffer[0] == 0xFF;
    Success &= ReadBuffer[1] == Command;

    if(!Success){
        Serial.printf("Failed to send command!\n");
        Serial.printf("Writebuffer: 0x%x 0x%x\n", WriteBuffer[0], WriteBuffer[1]);
        Serial.printf("ADC Command Buffer: 0x%x 0x%x\n", ReadBuffer[0], ReadBuffer[1]);
    }else{
        Serial.printf("Successful!\n");
        
    }
    Serial.println("---------------------------------------------------------");
    return Success;
}

and the Output:

Waiting for DRDY to be LOW
DRDY is LOW
---------------------------------------------------------
Sent Command: 0xF5 0x0
Received Response: 0xFF 0xF5
Successful!
---------------------------------------------------------
ADS1261 Initialization Started...

Sending RESET command...

---------------------------------------------------------
Sent Command: 0x6 0xAA
Received Response: 0xFF 0x7
Failed to send command!
Writebuffer: 0x6 0xaa
ADC Command Buffer: 0xff 0x7
---------------------------------------------------------
---------------------------------------------------------
Sent Command: 0xF5 0x0
Received Response: 0xFF 0xF5
Successful!
---------------------------------------------------------
Configuring ADC Registers...

---------------------------------------------------------
Sent Command: 0x43 0x2D
Received Response: 0xFF 0x43
Successful!
---------------------------------------------------------
---------------------------
Read Value: 0x2d
---------------------------
---------------------------------------------------------
Sent Command: 0x50 0x0
Received Response: 0xFF 0x51
Failed to send command!
Writebuffer: 0x50 0x0
ADC Command Buffer: 0xff 0x51
---------------------------------------------------------
---------------------------
Read Value: 0x1
---------------------------
---------------------------------------------------------
Sent Command: 0x46 0x10
Received Response: 0xFF 0x47
Failed to send command!
Writebuffer: 0x46 0x10
ADC Command Buffer: 0xff 0x47
---------------------------------------------------------
---------------------------
Read Value: 0x11
---------------------------
---------------------------------------------------------
Sent Command: 0x51 0x10
Received Response: 0xFF 0x51
Successful!
---------------------------------------------------------
---------------------------
Read Value: 0x11
---------------------------
Waiting for DRDY to be LOW...
DRDY is LOW
Failed to initialize ADC registers!

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Daniel、您好!

    我在你的代码中看到把/CS 设置为低电平来启动一个帧、但我没有看到任何将/CS 设置为高电平来结束该帧的代码。  /CS 可以保持低电平、但然后 ADC SPI 只会计数 SCLK、如果有任何其他 SCLK、通信将变得不同步。  额外的 SCLK 可能由固件问题或信号完整性问题引起、在这些问题上、时钟振铃和 ADC 会为每次转换解释多个 SCLK。

    您可能需要使用示波器来查看 SCLK、以确认波形干净且振铃最少。  构建代码结构以在每个帧的末尾将/CS 置于高电平、也可以改善通信。

    此外、如果您的控制器的逻辑电平与 ADC 不同、这也会导致通信问题。  请确认 ADS1261上的 DVDD 与您的控制器板上的 IO 电平匹配。  还请提供一些逻辑捕获的图片。

    此致、
    Keith Nicholas
    精密 ADC 应用

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    尊敬的 Keith:

    感谢您对/CS 的提示! 遗憾的是、这样无效。

    我用示波器检查了时钟信号、看上去一切正常、不是最佳的、而是正常工作。 我还检查了原理图、逻辑电平 DVDD 为3.3V、与控制器板相匹配。

    SPI 时钟:

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    Daniel、您好!

    SCLK 看起来相当干净;我想您测量的峰值是测量噪声、而不是 SCLK 上的实际噪声。  然而、如果您放大其中一个上升沿、这将有助于确认时钟边沿没有明显的振铃。

    您提到您已捕获逻辑波形、这些波形看起来是正确的。  许多逻辑分析仪都具有免费的查看器;如果您可以向我发送一个逻辑分析仪文件、该文件捕获正确的寄存器写入操作、后跟错误的寄存器写/回读操作、我将查看是否存在任何可能的时序问题。

    目标信号为 SCLK、DOUT、DIN、/CS 和/DRDY。

    此致、
    Keith