请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DLP4710 “线程”中讨论的其他部件:DLPA3005, DLPC3439
工具/软件:Linux
您好,
我想将DLPA3005的开机时间缩短到 可以控制 DLPC3439交换机源的时间。
通过实验,如果间隔太短,我无法 控制DLPC3439。
谢谢你
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.