工具/软件:
现在我无法打开具有 Raw10 3840x2160 30fps 的 IMX728 摄像头
这是 IMX728 的设置。 您能帮助我生成具有相同视频类型和帧大小的 Patten 吗? 验证问题所在。 非常感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具/软件:
现在我无法打开具有 Raw10 3840x2160 30fps 的 IMX728 摄像头
这是 IMX728 的设置。 您能帮助我生成具有相同视频类型和帧大小的 Patten 吗? 验证问题所在。 非常感谢
您好、Meng、
下面是用于生成所需分辨率的脚本:
board.WriteReg (0xB0、0x00)
board.WriteReg (0xB1、0x01)
board.WriteReg (0xB2、0x01)#enable 图形发生器
board.WriteReg (0xB1、0x02)
board.WriteReg (0xB2、0x33)#固定彩色条图形、8 个彩色条、
board.WriteReg (0xB1、0x03)
board.WriteReg (0xB2、0x2b)#CSI 数据标识符(0x24 = RGB888、0x2C = 12 位)
board.WriteReg (0xB1、0x04)
board.WriteReg (0xB2、0x12)#line Size (15:8)
board.WriteReg (0xB1、0x05)
board.WriteReg (0xB2、0xC0)#line Size (7:0)
board.WriteReg (0xB1、0x06)
board.WriteReg (0xB2、0x02) 条形码大小 (15:8)
board.WriteReg (0xB1、0x07)
board.WriteReg (0xB2、0x58)#bar 大小 (7:0)
board.WriteReg (0xB1、0x08)
board.WriteReg (0xB2、0x08) 每帧有效行数 (15:8)
board.WriteReg (0xB1、0x09)
board.WriteReg (0xB2、0x70) 每帧有效行数 (7:0)
board.WriteReg (0xB1、0x0a)
board.WriteReg (0xB2、0x08)#每帧总行数 (15:8)
board.WriteReg (0xB1、0x0B)
board.WriteReg (0xB2、0x9D)#每帧总行数 (7:0)
board.WriteReg (0xB1、0x0c)
board.WriteReg (0xB2、0x05)#line Period (15:8)
board.WriteReg (0xB1、0x0d)
board.WriteReg (0xB2、0xE8)#line Period (7:0)
board.WriteReg (0xB1、0x0E)
board.WriteReg (0xB2、0x21)#垂直后沿
board.WriteReg (0xB1、0x0F)
board.WriteReg (0xB2、0x0a)#垂直前沿