请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TFP410 大家好,团队
对于 TFP410,如何为 通用图形控制器接口选择1.1 V 至1.8 V 可调输入信号电平? 使用1.8V 电压时是否考虑因素?
非常感谢
马修·陈
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.