如果电源电压低于3.6V,TPS2064无法正确打开。 数据表指出,它应该用于2.7V和5.5V之间的电源电压。 如果电源电压为3.6V或更高,则在大约1.4V时将正确打开。 请建议解决方案? 我们需要它在3.3V电源电压下工作。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我正在发送项目的示意图: