请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TUSB7340
您好,
关于TUSB7340上的3.0 的各端口,我的客户正在询问问题。
每个3.0 是否只能通过寄存器禁用每个SCRX/TX_DN1-4端口?
我知道Portx_DIS寄存器可以禁用2.0 和3.0 端口。
但我无法找到仅禁用3.0 SCRX/TX_DNx端口的寄存器。
此致,
TAO_2199
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.