您好:先生,
我们使用SN65DP159芯片调整Windows XP GPU的视频信号输出,带宽为5.4Gbps (图像分辨率3840x2160.60Hz)2160.60),但从SN65DP159获得的用于显示的图像闪烁,似乎SN65dp159的信号不是很好,我们尝试通过编辑一些寄存器(如Reg0CH)来修复 和REG0x4D,但图像仍然不稳定,如何调整SN65DP159寄存器以提升信号质量以使图像稳定?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:先生,
我们使用SN65DP159芯片调整Windows XP GPU的视频信号输出,带宽为5.4Gbps (图像分辨率3840x2160.60Hz)2160.60),但从SN65DP159获得的用于显示的图像闪烁,似乎SN65dp159的信号不是很好,我们尝试通过编辑一些寄存器(如Reg0CH)来修复 和REG0x4D,但图像仍然不稳定,如何调整SN65DP159寄存器以提升信号质量以使图像稳定?
您好,Xuyu:
我方面有些困惑
对于超高清@60Hz,24bpp,4:4:4
HDMI要求5.94Gbps (三通道)
DP需要4.46Gbps (四通道)
我看到应用程序是DP159作为DP再定时器。
在x模式下,配置通过I2C完成,没有GPIO选项。
配置在第1页的寄存器中完成
配置脚本选择固定均衡器。
当您修改0x4D (EQFTC,EQLEV)中的值时,是否运行整个配置脚本?
当您修改EQLEV时,是否在寄存器0x33中更新EQ?
此致