Other Parts Discussed in Thread: TCA6507
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:TCA6507 您好,
产品页面显示 I/O 具有5V容限。 但根据数据表,SDA和SCL上的建议最大电压为3.6V。 所以我在这里有点困惑。
是否可以使用3.3V电源,并将SDA和SCL线路拉至5V?
谢谢,此致,
Frans Jan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.