请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DP8.3867万IR 您好,
DP8.3867万IR能否在晶体振荡器输入的25MHz以外的频率上运行? 如果没有,TI是否有任何以太网1000Base PHY可接受其它频率(如50MHz或125MHz)? (EMI问题)。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
DP8.3867万IR能否在晶体振荡器输入的25MHz以外的频率上运行? 如果没有,TI是否有任何以太网1000Base PHY可接受其它频率(如50MHz或125MHz)? (EMI问题)。